Reg: Compiling LTIB_Uboot error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: Compiling LTIB_Uboot error

ソリューションへジャンプ
1,898件の閲覧回数
vishvapathi
Contributor V

./ltib -m prep -p u-boot

Installing host support packages.

This only needs to be done once per host, but may take up to

an hour to complete ...

If an error occurs, a log file with the full output may be found in:

/home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log

Exiting on error or interrupt

Please see >> /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log for details

cat /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log

Updating lpp from local packages

+ cp -dp /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/pkgs/u-boot-2009.08 /opt/freescale/pkgs/u-boot-2009.08

cp: omitting directory `/home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/pkgs/u-boot-2009.08'

Died at ./ltib line 2518.

traceback:

main::check_dirs:2518

  main::host_checks:1438

   main:554

how to solve this issue??



ラベル(2)
0 件の賞賛
返信
1 解決策
1,693件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

After installed the LTIB, please run ./ltib first.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,694件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

After installed the LTIB, please run ./ltib first.

0 件の賞賛
返信