Refresh cycle counter in IPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Refresh cycle counter in IPU

ソリューションへジャンプ
1,990件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

From i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 4, 07/2018

38.1.2.1.6.1 Screen Refresh
• The refresh rate may vary within a predefined range. Within this range, the rate is
dynamically adjusted to the content update rate.
• An indication about the availability of new content is obtained as follows:

• If the page-flip double buffering is used, the mechanism provides this indication
• If only a single buffer is used (and incrementally updated), the IPU can receive
an indication of a modification from the ARM platform (by setting an internal
flag).
The IPU counts the refresh cycles: the total and those with new content. The ARM
platform can use these counters to optimize display management (e.g. switching
display buffer compression on/off). The counters are reset by the ARM platform.
• The transferred data may be processed on the way, using the IC and DP.

IPU is counting display refresh cycles according to above description.

I would like to check this counter for debugging our system.

Could you please teach me register name to get the counted value?

Best Regards,

Kazuma Sasaki.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,939件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kazuma Sasaki,

I made some research and the counter for refresh cycles is not accessible as it is part of the DP (Display Processor) and there is not a register from where this value could be read.

My apologies for the inconvenience.

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,940件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kazuma Sasaki,

I made some research and the counter for refresh cycles is not accessible as it is part of the DP (Display Processor) and there is not a register from where this value could be read.

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信
1,939件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hello gusarambula,

Okay, I got it. Thank you for your support.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信