Reduce DRAM and CPU frequency U-Boot in imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reduce DRAM and CPU frequency U-Boot in imx8mm

2,231 Views
Udhay_
Contributor III

I am working on power consumption in imx8mm and trying to reduce dram and cpu frequency.

Ex:

U-Boot SPL 2021.04-imx_v2021.04_5.15.5-1.0.0+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000)

DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done

Need to reduce DRAM rate 3000MTS To 1500MTS

Ex:

U-Boot 2021.04-imx_v2021.04_5.15.5-1.0.0+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000)

CPU: i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 34C

Need to reduce CPU frequency 1200 MHZ to 800 MHZ

is there anyone knows about how to decrease this?

Thanks in advance

0 Kudos
Reply
4 Replies

2,200 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

1.For new frequency of DRAM:

You need refer below guide to do stress test and generate new lprddr4_timing.c in this folder board/freescale/imx8mm_evk

 https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

2.For new CPU frequency 

Line 544 in this arch/arm/mach-imx/imx8m/clock_imx8mm.c

0 Kudos
Reply

2,192 Views
msharma
Contributor II

Hello Zhiming,
           The generated timming.c file gives the error while booting as mentioned above, However I have modified the .drate = 400 in the lpddr4_timming.c file and commented the remaining drates in the  dram_fsp_msg struct. 

While booting I got : 

                  DDRINFO: DRAM rate 800MTS. 

But there is very negligible change in the power, current reduced is 10mA.

Also, as you said I modified the  intpll_configure(ANATOP_ARM_PLL, MHZ(800));  in clock_imx8mm.c file  and enabled the powersaving mode in the menu configuration. But no considerable change in the power.
                 
               Can you please guide what else could be done in order to reduce the power consumption.

0 Kudos
Reply

2,175 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need generate correct timing.c with ddr tool.

 For reducing the power consumption, you can try to disable useless hardware driver on your board.

0 Kudos
Reply

2,137 Views
Udhay_
Contributor III

@Zhiming_Liu 

we have generated the lpddr4_timing.c file. the issue is that ddr tool is genrerating old version of ddr tool like u-boot imx_v2018.03_4.14.78_1.0.0_ga but we are using version 2021 u-boot.

or 

we required #include <asm/arch/imx8m_ddr.h> this file we can not able to find this file in my u-boot or any other resources

note : /* please replace #include <asm/arch/ddr.h> with #include <asm/arch/imx8m_ddr.h> */

we need updated ddr tool for u-boot-imx 

* Generated code from MX8M_DDR_tool
*
* Align with uboot version:
* imx_v2019.04_5.4.x and above version
* For imx_v2018.03_4.14.78_1.0.0_ga ~ imx_v2018.04_4.19.35_1.1.0_ga:
* please replace #include <asm/arch/ddr.h> with #include <asm/arch/imx8m_ddr.h>

0 Kudos
Reply