Using i.mx8mp isi to convert raw10 to raw8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using i.mx8mp isi to convert raw10 to raw8

1,109件の閲覧回数
454799790
Contributor I

Hi NXP community,

I am using a sensor which can only output mipi raw10 format,but I need a raw8 format.

Can I use the isi to convert raw10 to raw8?

Thanks.

0 件の賞賛
返信
2 返答(返信)

1,067件の閲覧回数
454799790
Contributor I

Or can the mipi csi recevier do this?We don't want to convert raw10 to raw8 by cpu,it's too slow.

0 件の賞賛
返信

1,016件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @454799790 ,

I hope you are doing well.

RAW format input is copied into memory without any pixel change in ISI.

Please refer to 6.3.2 i.MX 8MN/i.MX 8MP ISI configuration in i.MX 8M Series MIPI Capture System for more information.

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信