Recompiling MFGTool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,522件の閲覧回数
Maddis
Contributor IV

Hi,

We have custom iMX6Q based HW. I remember last time it being really pain to get MFGTool recompiled but somehow I managed.

Now there was modification to HW and I need to update MFGTool Linux system as well. I managed to get it compiled and it boots but always stops at this:

ALSA device list:
No soundcards found.
Freeing unused kernel memory: 736K (80cee000 - 80da6000)
Starting UTP
uuc 0.5 [built Aug 24 2017 06:21:04]
UTP: Waiting for device to appear

UTP: file/device node /dev/utp already exist

cpu_id is 0

Nothing happens after that. 

I'm using Yocto 2.2 (morty) and latest meta-freescale - layer version. Linux kernel version is 4.1.15

I made sure that I was using the imx_v7_mfg_defconfig stated in the manual but that didn't help any. 

Has anyone managed to recompile mfgtools with Yocto 2.1 or 2.2 or any idea what might be the problem?

This is the same problem I was having with the older 3.10.17 kernel based Yocto, but there I got it sorted someway. I just don't remember anymore how.

ラベル(3)
0 件の賞賛
返信
1 解決策
2,329件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mc

this may be caused by low usb_id pin as on

https://community.nxp.com/thread/365690
https://community.nxp.com/thread/375912

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,330件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mc

this may be caused by low usb_id pin as on

https://community.nxp.com/thread/365690
https://community.nxp.com/thread/375912

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,329件の閲覧回数
Maddis
Contributor IV

This was in fact the case! I went through the device tree and fixed the pin and now the mfgtool system boots and update starts!

0 件の賞賛
返信