Recommended connection when not used LICELL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommended connection when not used LICELL

ソリューションへジャンプ
2,069件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Let me confirm about recommended connection for LICELL in PF3000.

1.

I found the following document which describe about recommended connection for PF0100.

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf?fasp=1&WT_TYPE=Application%20Notes&W...

Can the recommended connection also apply for PF3000 ?

2.

According to the Table 1 of AN4717, NXP recommended user to connect "Bypass with 0.1 μF" when not used LICELL.

In my understanding this mean "Bypass with 0.1 μF to ground".

Is it correct ?

Ko-hey

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
1,940件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, you're right, just bypass through 0.1 μF to ground

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,941件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, you're right, just bypass through 0.1 μF to ground

0 件の賞賛
返信
1,940件の閲覧回数
ko-hey
Senior Contributor II

Hi

Thanks!

Ko-hey

0 件の賞賛
返信