Recommendation of DDR3L-SDRAM with i.MX6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommendation of DDR3L-SDRAM with i.MX6SL

ソリューションへジャンプ
1,520件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I have a question about recommendation of the DDR3L-SDRAM with i.MX6SL and have referred following communities.

https://community.freescale.com/message/574596#574596

https://community.freescale.com/message/485528#485528

My customer plan to use four chips DDR3L-SDRAM with i.MX6SL.

However, we can't find recommended description and information of DDR3L-SDRAM in IMX6SLHDG.

Is the recommendation same as DDR3-SDRAM ?

If not, please let us a recommendation.

In the first place, can we use four chips DDR3L-SDRAM with i.MX6SL ?

Ko-hey

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,331件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

design recommendations are the same as for DDR3-SDRAM.

Yes one can use four chips DDR3L-SDRAM with i.MX6SL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,332件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

design recommendations are the same as for DDR3-SDRAM.

Yes one can use four chips DDR3L-SDRAM with i.MX6SL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,331件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

OK, Thanks !

Ko-hey

0 件の賞賛
返信