Recommendation of DDR3L-SDRAM with i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommendation of DDR3L-SDRAM with i.MX6SL

Jump to solution
1,517 Views
ko-hey
Senior Contributor II

Hi all

I have a question about recommendation of the DDR3L-SDRAM with i.MX6SL and have referred following communities.

https://community.freescale.com/message/574596#574596

https://community.freescale.com/message/485528#485528

My customer plan to use four chips DDR3L-SDRAM with i.MX6SL.

However, we can't find recommended description and information of DDR3L-SDRAM in IMX6SLHDG.

Is the recommendation same as DDR3-SDRAM ?

If not, please let us a recommendation.

In the first place, can we use four chips DDR3L-SDRAM with i.MX6SL ?

Ko-hey

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

design recommendations are the same as for DDR3-SDRAM.

Yes one can use four chips DDR3L-SDRAM with i.MX6SL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,329 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

design recommendations are the same as for DDR3-SDRAM.

Yes one can use four chips DDR3L-SDRAM with i.MX6SL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,328 Views
ko-hey
Senior Contributor II

Hi Igor

OK, Thanks !

Ko-hey

0 Kudos
Reply