Recommendation for Camera Module with Integrated ISP for i.MX93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Recommendation for Camera Module with Integrated ISP for i.MX93

2,077 次查看
ItamarEliakim
Contributor I

Hi,

I'm working with the i.MX93 processor, which lacks an onboard ISP. I'm looking for recommendations on camera modules similar to the OV5640, providing integrated ISP capabilities such as automatic brightness, auto white balance, and exposure control.

Ideally, the module should be easy to integrate with minimal additional processing required on the i.MX93 side.

Any suggestions or experiences would be highly appreciated.

Thanks!

标记 (3)
0 项奖励
回复
2 回复数

2,044 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,984 次查看
ItamarEliakim
Contributor I

Thanks for the suggestion, but the OV5640 is deprecated, and I’m looking for a newer sensor with 7 to 10 years of longevity. Do you have any recommendations for a camera module with an integrated ISP that would be a good fit for the i.MX93?

Appreciate your help!

Best,
Itamar

0 项奖励
回复