Recommendation for Camera Module with Integrated ISP for i.MX93

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommendation for Camera Module with Integrated ISP for i.MX93

2,018件の閲覧回数
ItamarEliakim
Contributor I

Hi,

I'm working with the i.MX93 processor, which lacks an onboard ISP. I'm looking for recommendations on camera modules similar to the OV5640, providing integrated ISP capabilities such as automatic brightness, auto white balance, and exposure control.

Ideally, the module should be easy to integrate with minimal additional processing required on the i.MX93 side.

Any suggestions or experiences would be highly appreciated.

Thanks!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,985件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,925件の閲覧回数
ItamarEliakim
Contributor I

Thanks for the suggestion, but the OV5640 is deprecated, and I’m looking for a newer sensor with 7 to 10 years of longevity. Do you have any recommendations for a camera module with an integrated ISP that would be a good fit for the i.MX93?

Appreciate your help!

Best,
Itamar

0 件の賞賛
返信