Reboot kernel,bootrom does not update boot config status.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reboot kernel,bootrom does not update boot config status.

1,248件の閲覧回数
echozeng
Contributor III

     Imx6q linux 3.0.35

     Switch boot config to sd3, as kernel is loaded from sd3 and then change boot config to sd4, reboot system, the  system      load from sd3 again.

     Why does not bootrom  update boot cofig status? 

     If provide POR_B pin  reset sequence, the same result as uper description.

ラベル(2)
0 件の賞賛
返信
1 返信

1,143件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please check the boot configuration, using SRC_SBMR1 register.

Also, please verify U-boot environment, where kernel, rootfs are really located.

Only POR provides BOOT_MODE and BOOT_CFG re-read.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信