Reboot kernel,bootrom does not update boot config status.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reboot kernel,bootrom does not update boot config status.

910 次查看
echozeng
Contributor III

     Imx6q linux 3.0.35

     Switch boot config to sd3, as kernel is loaded from sd3 and then change boot config to sd4, reboot system, the  system      load from sd3 again.

     Why does not bootrom  update boot cofig status? 

     If provide POR_B pin  reset sequence, the same result as uper description.

标签 (2)
0 项奖励
回复
1 回复

805 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please check the boot configuration, using SRC_SBMR1 register.

Also, please verify U-boot environment, where kernel, rootfs are really located.

Only POR provides BOOT_MODE and BOOT_CFG re-read.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复