Reassigned pin power group

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reassigned pin power group

Jump to solution
1,811 Views
faiz
Contributor I

Hello,

On our board, we have UART power group (NVCC_UART) connected to 1.8V and SPI power group (NVCC_ECSPI) connect to 3.3V. 

We want to reassign ECSPI1_SCLK (D6) and ECSPI1_MOSI (B7) to UART3.RX and UART3.TX. Would the voltage group be 3.3V or 1.8V? 

Thanks,
Faiz

Labels (1)
0 Kudos
Reply
1 Solution
1,770 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    i.MX8Mm pins ECSPI1_SCLK (D6) and ECSPI1_MOSI (B7) belong to NVCC_ECSPI power group,

therefore the mentioned UART signal will be under 3.3V.

Use the i.MX Pins tool.

Pins Tool for i.MX Application Processors | NXP 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
1 Reply
1,771 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    i.MX8Mm pins ECSPI1_SCLK (D6) and ECSPI1_MOSI (B7) belong to NVCC_ECSPI power group,

therefore the mentioned UART signal will be under 3.3V.

Use the i.MX Pins tool.

Pins Tool for i.MX Application Processors | NXP 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply