Real Time Edge Software in imx8 question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Real Time Edge Software in imx8 question

1,854件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

NXP release the real-time-edge-software.

Follow the User-Guide and Yocto Project Guide.

Our BSP is Yocto 3.3 and kernel version is 5.10.35.  

How to do porting the Real-time Edge Yocto?

(1) In Edge Software 2.0,  Linux 5.10.9-rt24 is the base of Linux kernel.

(2) In Edge Software 2.1,  Linux 5.10.52-rt47 is the base of Linux kernel.

Our Current BSP (kernel version) does not match.

Do you have any advice?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,847件の閲覧回数
jim_lin
NXP Employee
NXP Employee

Hello Charles,

 

if you don't plan to port on your own, or don't have the resources to do so, 

you can contact NXP profession support or other software 3rd parties you preferred for the porting.

 

Best regards,

Jim

0 件の賞賛
返信

1,809件の閲覧回数
charleshuang
Senior Contributor II

Hello NXP and NXP(Jim)

The Demo Image  from https://www.nxp.com/design/software/development-software/real-time-edge-software:REALTIME-EDGE-SOFTW....

Real Time Edge Software v2.2 for IMX8MM

I cannot boot up on imx8MM Demo Board. Please help to check it. Thanks.

 

 

 

 

タグ(2)
0 件の賞賛
返信