Real Time Edge Software in imx8 question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Real Time Edge Software in imx8 question

1,798 Views
charleshuang
Senior Contributor II

Hi NXP Team

NXP release the real-time-edge-software.

Follow the User-Guide and Yocto Project Guide.

Our BSP is Yocto 3.3 and kernel version is 5.10.35.  

How to do porting the Real-time Edge Yocto?

(1) In Edge Software 2.0,  Linux 5.10.9-rt24 is the base of Linux kernel.

(2) In Edge Software 2.1,  Linux 5.10.52-rt47 is the base of Linux kernel.

Our Current BSP (kernel version) does not match.

Do you have any advice?

0 Kudos
Reply
2 Replies

1,791 Views
jim_lin
NXP Employee
NXP Employee

Hello Charles,

 

if you don't plan to port on your own, or don't have the resources to do so, 

you can contact NXP profession support or other software 3rd parties you preferred for the porting.

 

Best regards,

Jim

0 Kudos
Reply

1,753 Views
charleshuang
Senior Contributor II

Hello NXP and NXP(Jim)

The Demo Image  from https://www.nxp.com/design/software/development-software/real-time-edge-software:REALTIME-EDGE-SOFTW....

Real Time Edge Software v2.2 for IMX8MM

I cannot boot up on imx8MM Demo Board. Please help to check it. Thanks.

 

 

 

 

Tags (2)
0 Kudos
Reply