Read back bootable image from FlexSPI NOR flash and save as hex file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Read back bootable image from FlexSPI NOR flash and save as hex file

710 次查看
kennethkong852
Contributor II

Hello!

Board = RT1060-EVKB (eventually migrate to a custom hardware with RT1062 MCU)

Using tool like MCU Boot Utility (or even cmd line tool like blhost), is there a way that I can backup/readback the bootable image contents (e.g. 0x60000000 to 0x60006000) in my FlexSPI NOR flash to a valid .hex file?

I have used MCU Boot Utility GUI but that does not give me a .hex file when reading back...

From there, ideally I would like to merge part of this hex file with a raw application image... this is all for development purposes.

Any help or guidance on the above would be greatly appreciated!

BEST REGARDS,

KENNETH

标签 (1)
0 项奖励
回复
1 回复

658 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I review the Secure provisioning tool, but this does not have this option available. Maybe you could use the BLHOST but that tool needs to specify the address and the size, but this does not have the option to sabe in hex.

Best regards,
Pavel

0 项奖励
回复