Re: imx6q debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: imx6q debug

Jump to solution
1,482 Views
wangcuixmwangcu
Contributor III
  • "Hardware-bring up:

     Check the power, power sequence, clock, reset, provide the boot configuration to software, run ddr test."

     

Only boot configuration, can a DDR test?
1 Solution
1,426 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the DDR Stress test (bare metal) :

https://community.nxp.com/docs/DOC-105652 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,427 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the DDR Stress test (bare metal) :

https://community.nxp.com/docs/DOC-105652 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------