Re: imx6q debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,425件の閲覧回数
wangcuixmwangcu
Contributor III
  • "Hardware-bring up:

     Check the power, power sequence, clock, reset, provide the boot configuration to software, run ddr test."

     

Only boot configuration, can a DDR test?
1 解決策
1,369件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the DDR Stress test (bare metal) :

https://community.nxp.com/docs/DOC-105652 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,370件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the DDR Stress test (bare metal) :

https://community.nxp.com/docs/DOC-105652 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------