Re: i.MX6ULL Watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: i.MX6ULL Watchdog

3,154 Views
bimal
Contributor III

Hi,

Thanks for reply,

I have referred to EVK boards, but i don't want to use inbetween Voltage supervisor IC.

Instead of this i want to give the WDOG_Any pin to nPOR input of i.mx6ULL processor.

Here my concern is whether POR will be able to detect the pulse of WDOG_Any pin?

Also i would like to get info that whether the internal Software reset signal will restart i.mx6ull processor(which is generated after watchdog timer expires) ?

0 Kudos
Reply
1 Reply

803 Views
Yuri
NXP Employee
NXP Employee

Hello,


  It is highly recommended to remove power (voltage source) of all

components on the board in the event of a processor reset in order

to avoid i.MX SoC boot issues when power not removed during reset.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply