Re: how to bring up CSI_1 interface in parallel mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: how to bring up CSI_1 interface in parallel mode

2,424 次查看
GopiNagaBharath
Contributor IV

I am also using the CSI1 port of i.MX53 with the TI Video Decoder TVP5147M1 for interfacing the PAL output Camera.

When we run the camera test command, we are just getting the first frame on the display, instead of getting the stream.

Also, we are getting the below errors in the debug window.

------------------------------------------------------------------------

Detected screen resolution is 640 x 480

main[711] #1

main[734] #2

main[738] #3

IPU:In csi_enc_enabling_tasks

In csi_enc_setup

main[745] #4

main[780] #5

mxc_ipu mxc_ipu: warning: disable ipu dma channel 0 during its busy state

IPU:In csi_enc_enabling_tasks

In csi_enc_setup

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00000001

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

fd_capture_v4l : VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

fd_capture_v4l: VIDIOC_QBUF failed

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

fd_capture_v4l : VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

fd_capture_v4l: VIDIOC_QBUF failed

mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001

mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

fd_capture_v4l : VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

fd_capture_v4l: VIDIOC_QBUF failed

-------------------------------------------------------------------------------------------------------

Any idea what could be the issue???

Thanks!

0 项奖励
回复
4 回复数

1,807 次查看
linyang1
Contributor I

Hi, have you solved this issue? Or have some advice?

0 项奖励
回复

1,807 次查看
GopiNagaBharath
Contributor IV

Hello Lin Yang,

We have still not resolved this issue. For time being, we are using as USB based capture device (EasyCAP) for video streaming. We are suffering with high CPU usage to stream & capture the video with this capture device.

Regards,

Gopi

0 项奖励
回复

1,807 次查看
linyang1
Contributor I

Thanks for your reply!My issue is because of hardware data lane.It's resolved.

0 项奖励
回复

1,807 次查看
GopiNagaBharath
Contributor IV

Are you using the port CSI1 or CSI0?

I am trying to capture the video from TVP5147M1 (on evaluation kit), but when it is captured, I am having two frames coming as a single frame.

Were you able to get the TVP5147M1 work for streaming the video?

0 项奖励
回复