I am also using the CSI1 port of i.MX53 with the TI Video Decoder TVP5147M1 for interfacing the PAL output Camera.
When we run the camera test command, we are just getting the first frame on the display, instead of getting the stream.
Also, we are getting the below errors in the debug window.
------------------------------------------------------------------------
Detected screen resolution is 640 x 480
main[711] #1
main[734] #2
main[738] #3
IPU:In csi_enc_enabling_tasks
In csi_enc_setup
main[745] #4
main[780] #5
mxc_ipu mxc_ipu: warning: disable ipu dma channel 0 during its busy state
IPU:In csi_enc_enabling_tasks
In csi_enc_setup
mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00000001
mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
fd_capture_v4l : VIDIOC_DQBUF failed.
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
fd_capture_v4l: VIDIOC_QBUF failed
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
fd_capture_v4l : VIDIOC_DQBUF failed.
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
fd_capture_v4l: VIDIOC_QBUF failed
mxc_ipu mxc_ipu: Channel already disabled 10
mxc_ipu mxc_ipu: Channel already uninitialized 10
mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001
mxc_ipu mxc_ipu: Channel already disabled 10
mxc_ipu mxc_ipu: Channel already uninitialized 10
mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x00000001
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
fd_capture_v4l : VIDIOC_DQBUF failed.
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
fd_capture_v4l: VIDIOC_QBUF failed
-------------------------------------------------------------------------------------------------------
Any idea what could be the issue???
Thanks!
Hi, have you solved this issue? Or have some advice?
Hello Lin Yang,
We have still not resolved this issue. For time being, we are using as USB based capture device (EasyCAP) for video streaming. We are suffering with high CPU usage to stream & capture the video with this capture device.
Regards,
Gopi
Thanks for your reply!My issue is because of hardware data lane.It's resolved.
Are you using the port CSI1 or CSI0?
I am trying to capture the video from TVP5147M1 (on evaluation kit), but when it is captured, I am having two frames coming as a single frame.
Were you able to get the TVP5147M1 work for streaming the video?