Re: Time model for the MCIMX6S7CVM08AC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Time model for the MCIMX6S7CVM08AC

ソリューションへジャンプ
920件の閲覧回数
sesmor
Contributor II

Hi Yuri,
 I had created the request to get time model, but I have got time model for DDR3l-1066 instead of DDR3l-800. I was trying to create this model by myself and i was using JEDEC standarts called JESD79‐3‐1A.01 and  JESD79-3C. Do that documents content correct time characteristics for speed grade 800?

0 件の賞賛
返信
1 解決策
875件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  generally - yes, You may rely on the JEDEC docs. Strictly speaking, i.MX6 MMDC 

is based on JESD79-3D DDR3 JEDEC standard release.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
876件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  generally - yes, You may rely on the JEDEC docs. Strictly speaking, i.MX6 MMDC 

is based on JESD79-3D DDR3 JEDEC standard release.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------