Re: Linux iMX6 PCIe driver not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Linux iMX6 PCIe driver not working

1,119 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please check PCIe clock configuration.

HW Design Checking List for i.Mx6DQSDL Rev2.9 contains useful recommendations

about using (external) PCIe clock :

"Due to CLKx_P/N is LVDS port and don't match with PCIe reference clock specification.

For PCIe Gen1 application, following low cost solution can be used(DC bias and AC

impedance should be considered).  Please refer to "HW Design Checking List for i.Mx6DQSDL

Rev2.7.xlsx", sheet "Schematic", Ref12 for more info."

  "PCIe reference clock solution which provided by CLKx_N/P of i.MX6 chip can't pass PCIe

Gen2 compliance test.  Recommend using external PCIe 2.0/3.0 clock generator with 2 HCSL

outputs solution. One clock channel connect to i.MX6 as a reference input, please click

Ref14 ("HW Design Checking List for i.Mx6DQSDL Rev2.9.xlsx") for reference circuit.

Another clock channel should connect to PCIe connector, please contact generator vendor

for detailed design guide."

HW Design Checking List for i.MX6DQSDL 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
0 Replies