Re: How to build the yocto SDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: How to build the yocto SDK?

ソリューションへジャンプ
2,009件の閲覧回数
rans
Senior Contributor I

Hello Yuri,

I am trying to popluate sdk with the command you've given:

bitbake core-image-minimal -c populate_sdk

But I wander:

if populate_sdk is one of the tasks in  core-image-minimal , doesn't it mean it should have already been executed in the first run of bitbake ?

Thanks,

Ran

0 件の賞賛
返信
1 解決策
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   the "-c" option is used to instruct bitbake just to execute the populale_sdk task.

Also You may look at 

https://community.nxp.com/docs/DOC-334814 

Regards,

Yuri.

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,436件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   the "-c" option is used to instruct bitbake just to execute the populale_sdk task.

Also You may look at 

https://community.nxp.com/docs/DOC-334814 

Regards,

Yuri.

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信