Re: How to build the yocto SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: How to build the yocto SDK?

Jump to solution
2,014 Views
rans
Senior Contributor I

Hello Yuri,

I am trying to popluate sdk with the command you've given:

bitbake core-image-minimal -c populate_sdk

But I wander:

if populate_sdk is one of the tasks in  core-image-minimal , doesn't it mean it should have already been executed in the first run of bitbake ?

Thanks,

Ran

0 Kudos
Reply
1 Solution
1,440 Views
Yuri
NXP Employee
NXP Employee

Hello,

   the "-c" option is used to instruct bitbake just to execute the populale_sdk task.

Also You may look at 

https://community.nxp.com/docs/DOC-334814 

Regards,

Yuri.

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
Reply
1 Reply
1,441 Views
Yuri
NXP Employee
NXP Employee

Hello,

   the "-c" option is used to instruct bitbake just to execute the populale_sdk task.

Also You may look at 

https://community.nxp.com/docs/DOC-334814 

Regards,

Yuri.

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply