RTC doesn't works properly with HAL enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC doesn't works properly with HAL enabled

1,316件の閲覧回数
stefano6641
Contributor I

Good morning,

  I have some problems with my iMX 1021 board with HAL enabled. The application failed to write HPRC register in SNVS bank, no error reported but data aren't set.

The same binary file, loaded on a bord without HAL active, works properly.

 

Some help?

Thanks,

Stefano

0 件の賞賛
返信
3 返答(返信)

1,303件の閲覧回数
stefano6641
Contributor I

Another addiction: I can write in HPRC register just under boot, for some time. After that I can't do it. I'm not sure which condition lock the write on HPRC register.

 

BR,

Stefano

0 件の賞賛
返信

1,312件の閲覧回数
stefano6641
Contributor I

In addiction seems that LP_SEC_VIO and SV1 bits of HPSVSR register are high.

0 件の賞賛
返信

1,285件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, sorry for the later reply.

I am not sure if you refer the MCUXpresso SDK example <snvs_hp_rtc> for RT1020?

Mike

0 件の賞賛
返信