RTC doesn't works properly with HAL enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTC doesn't works properly with HAL enabled

1,884 次查看
stefano6641
Contributor I

Good morning,

  I have some problems with my iMX 1021 board with HAL enabled. The application failed to write HPRC register in SNVS bank, no error reported but data aren't set.

The same binary file, loaded on a bord without HAL active, works properly.

 

Some help?

Thanks,

Stefano

0 项奖励
回复
3 回复数

1,871 次查看
stefano6641
Contributor I

Another addiction: I can write in HPRC register just under boot, for some time. After that I can't do it. I'm not sure which condition lock the write on HPRC register.

 

BR,

Stefano

0 项奖励
回复

1,880 次查看
stefano6641
Contributor I

In addiction seems that LP_SEC_VIO and SV1 bits of HPSVSR register are high.

0 项奖励
回复

1,853 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, sorry for the later reply.

I am not sure if you refer the MCUXpresso SDK example <snvs_hp_rtc> for RT1020?

Mike

0 项奖励
回复