RT685 Flexcomm design rule.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT685 Flexcomm design rule.

1,478 次查看
StephenYeh
Contributor III

Hi Sir

Does the RT685 Flexcomm feature support SPI(MOSI) and GPIO?

 If my system only needs MOSI, and the MISO/SS pin can set to GPIO pin.

 

 

0 项奖励
回复
3 回复数

1,457 次查看
StephenYeh
Contributor III

Hi Sir,

Thanks.

If I want to share the Flexcomm0 for SPI and I2C @rtos. (It needs re-initial the pin define)

Because our system have many I2C device(same slave address).

Do you recommend this design?

 

0 项奖励
回复

1,451 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

It is possible to share the Flexcomm interface, but as you mentioned you will have to reconfigure the interface to switch between protocols. It will depend on the application if this can affect the desired performance.

Best regards, Daniel.

0 项奖励
回复

1,462 次查看
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Flexcomm interface supports the following features:

DanielRuvalcaba_0-1661294656398.png

It does support SPI.

For more information, you can refer to chapter 21 of the UM.

I hope this helps, Daniel.

0 项奖励
回复