RT685 Flexcomm design rule.

cancel
Showing results for 
Search instead for 
Did you mean: 

RT685 Flexcomm design rule.

281 Views
StephenYeh
Contributor III

Hi Sir

Does the RT685 Flexcomm feature support SPI(MOSI) and GPIO?

 If my system only needs MOSI, and the MISO/SS pin can set to GPIO pin.

 

 

0 Kudos
3 Replies

260 Views
StephenYeh
Contributor III

Hi Sir,

Thanks.

If I want to share the Flexcomm0 for SPI and I2C @rtos. (It needs re-initial the pin define)

Because our system have many I2C device(same slave address).

Do you recommend this design?

 

0 Kudos

254 Views
DanielRuvalcaba
NXP Employee
NXP Employee

Hi,

It is possible to share the Flexcomm interface, but as you mentioned you will have to reconfigure the interface to switch between protocols. It will depend on the application if this can affect the desired performance.

Best regards, Daniel.

0 Kudos

265 Views
DanielRuvalcaba
NXP Employee
NXP Employee

Hi,

Flexcomm interface supports the following features:

DanielRuvalcaba_0-1661294656398.png

It does support SPI.

For more information, you can refer to chapter 21 of the UM.

I hope this helps, Daniel.

0 Kudos