RT1064 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 EVK

1,318 Views
vishwas_br
Contributor II

We are using RT1064 in Internal boot mode and MCUXpresso Secure Provisioning tool. After writing image (bootloader file) is successful and re-energizing the board, the device is in bootloader mode. Further, flashing is not possible, connection is not possible. Programming is possible only once and then the chip needs to be erased using debugger, in order to go forward. Is there an option available or any software to erase without using debugger or currently present in MCUXpresso Secure Provisioning tool? Is there any reset condition available for flashing operation? Kindly help

0 Kudos
Reply
1 Reply

1,302 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vishwas_br ,

  Reset condition to do the erase is not OK.

  Your issue is caused by the invalid app is downloaded to the flash, the the boot is not work, the core can't find the valid entrypoint.

  The solution is do the flash erase, normally, we use the serial download mode to do the mass erase, or the debugger do the mass erase.

  If you use the JLINK, you also can use the JLINK commander, erase all.

  Anyway, still need the debugger, or the serial download mode, then the blhost will help you, blhost also be used in the SPT tool, that's why you make it works, you also can use the MCUbootutility tool in serail download mode.

  Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply