RT 120 Firmware update using Flashloader (continuation of https://community.nxp.com/thread/494337)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT 120 Firmware update using Flashloader (continuation of https://community.nxp.com/thread/494337)

1,736 Views
ashishpradhan
Contributor II

We tried the USB option too. That did not work either.

We would like to do the firmware update via UART. The flash loader documentation does mention it supported both USB and UART. Did we miss something?

0 Kudos
Reply
1 Reply

1,572 Views
Yuri
NXP Employee
NXP Employee

Hello,

   from the app team:

   RT1020 has different downloading and jumping addresses for ivt_flashloader.bin, they are 0x20208000 and 0x20208400. 

   For the AN12238, it just gives the descriptions of the general Flashloader information, includes the common knowledge, steps and commands, and selects the RT1050 platform as the example.

Regards,

Yuri.