imx6 quad thermal analysis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 quad thermal analysis

1,294件の閲覧回数
abhaykumar_sing
Contributor I

Hi,

I need to perform thermal analysis for IMX6 Quad core.

How can i enable and stress all applicable peripherals and also Is there some Stress Tool available to Stress the Cores of the IMX6 processor?

0 件の賞賛
返信
1 返信

1,239件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi abhay

unfortunately such special tools or images are not available.

In general one can try Demo image with a gui from below link

and run some high resolution video or graphics, this will stress

most of processor peripherals

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信