RPM built error while running ltib

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RPM built error while running ltib

1,302 次查看
sarathsanthoss
Contributor I

Hi folks,

            I am getting the following issue while running ./ltib on ubuntu12.04

RPM build errors:

    Bad exit status from /home/giritharan/extra/ltib/tmp/rpm-tmp.74178 (%build)

Build time for u-boot-v2009.08: 0 seconds

Failed building u-boot-v2009.08

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu Oct 22 19:03:41 2015

Ended:   Thu Oct 22 19:03:43 2015

Elapsed: 2 seconds

These packages failed to build:

u-boot-v2009.08

Build Failed

Exiting on error or interrupt

thanks in advance..................

Message was edited by: sarathkumar natarajan

标签 (1)
0 项奖励
回复
2 回复数

1,186 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sarathkumar

it is necessary to install patches for ubuntu 12.04

Re: What are all the patches need it for LTIB on ubuntu 12.04

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,186 次查看
sarathsanthoss
Contributor I

thanks its woked

0 项奖励
回复