Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

3,131 次查看
ferdi
Contributor I

Hi :

Under the Linux3.0.35 kernel version, how to increase the access frequencies of IMX6Q SPI's CS ? The attachment is the picture of SPI access frequencies when clock cycles is 20 MHZ. Red one is CS singal,the yellow one is SPI clock signal.

Ferdi

Best Regards!

标签 (2)
0 项奖励
回复
2 回复数

2,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ferdi

one can try to enable dma:

https://community.freescale.com/thread/328465

https://lkml.org/lkml/2014/9/15/1075

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,961 次查看
ferdi
Contributor I

Dear igorpadykov:

     The connection patch is based on the IMX51 platform, which is not compatible with the IMX6Q platform, Do not know if there is a Linux3.0.35 based IMX6Q patch platform? Thank you!

Best regards!

Ferdi

0 项奖励
回复