RMII interface on i.mx6 Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RMII interface on i.mx6 Solo

8,146 Views
alexberenshtein
Contributor III

We use i.mx6 - Solo. We changed interface from RGMII to RMII. We use Marvell 88E6020 ,  have 2 steps.

1. In U-Boot:

MX6_PAD_ENET_MDIO__ENET_MDIO|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_MDC__ENET_MDC|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_CRS_DV__ENET_RX_EN|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_RX_ER__ENET_RX_ER|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_TX_EN__ENET_TX_EN|MUX_PAD_CTRL(ENET_PAD_CTRL), MX6_PAD_ENET_RXD0__ENET_RX_DATA0|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_RXD1__ENET_RX_DATA1|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_TXD0__ENET_TX_DATA0|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_ENET_TXD1__ENET_TX_DATA1|MUX_PAD_CTRL(ENET_PAD_CTRL) , MX6_PAD_GPIO_16__ENET_REF_CLK|MUX_PAD_CTRL(0x4001b0a8),

Working OK !!!!!!;

In kernel 4.1.15:
pinctrl_enet:

                enetgrp { fsl,pins =

< MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0

  MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0

 MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN

 0x1b0b0 MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER

 0x1b0b0 MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN

 0x1b0b0 MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0

 0x1b0b0 MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1

  0x1b0b0 MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0

 0x1b0b0 MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b0b0

  MX6QDL_PAD_GPIO_16__ENET_REF_CLK  0x4001b0a8 >;

};

pinctrl_enet_irq: enetirqgrp

 { fsl,pins = < MX6QDL_PAD_NANDF_ALE__GPIO6_IO08 0x000b1 >; }

Clock we get from MARVELL (50Mgz).

#define  MX6QDL_PAD_GPIO_16__ENET_REF_CLK   0x214 0x5e4 0x80c 0x12 0x0

Clear Bit 21 -> IOMUXC_GPR1[21] , Clock from Marvell !!!

 regmap_update_bits(gpr, IOMUXC_GPR1,IMX6Q_GPR1_ENET_CLK_SEL_MASK,0);

But , we get a message:  fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:18, irq=-1) IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready done.


What a problem ?

0 Kudos
Reply
6 Replies

7,072 Views
alexberenshtein
Contributor III

Hi Igor.

I see on terminal:

[    8.781755] fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch
[    8.791175] libphy: PHY fixed-0:00 not found
[    8.797571] fec 2188000.ethernet eth0: could not attach to PHY

Best regards

0 Kudos
Reply

7,070 Views
igorpadykov
NXP Employee
NXP Employee
Hi Alex

one can debug it, starting from probe function, please use attached

Linux Manual and AN4553 Using Open Source Debugging Tools forLinux on i.MX Processors

http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf 

linux-2.6.35.3-imx28/mv88e6020.c at master · embeddedarm/linux-2.6.35.3-imx28 · GitHub 

nxp has service for helping porting drivers: NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 Kudos
Reply

7,070 Views
alexberenshtein
Contributor III

Hi Igor.

Yes.

phy gpio reset is is  working good    0 / 1.

We get clock from Marvel.

bit GPR[21]=0 ---> Get clock from external .

IOMUXC_SW_MUX_CTL_PAD_GPIO16 ---> address 20E0214h

bit SION =1 -> ENABLED — Force input path of pad GPIO_16

MUX_MODE -> 010 (ALT2) -> select signal ENET_REF_CLK

About patch - I use kernel 4.1.15 - with all patches.

Best regards.

0 Kudos
Reply

7,069 Views
alexberenshtein
Contributor III

Hi Igor.

Yes.

We have :

 dts file in RMII  :

&fec { ..     phy-mode = "rmii";

MAC is OK.
0 Kudos
Reply

7,070 Views
igorpadykov
NXP Employee
NXP Employee
Hi Alex

is there phy gpio reset, is it working properly
&fec {.. 
MX6_enet_RMII.zip on 
 https://community.nxp.com/thread/304346?commentID=331971#comment-331971      

Best regards
igor

0 Kudos
Reply

7,070 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

has dts file rmii entry as in examples:

&fec { ..     phy-mode = "rmii";

linux-2.6-imx.git - Freescale i.MX Linux Tree 

https://community.nxp.com/message/841332?commentID=841332#comment-841332 

also one can check mac address as in attached Linux Manual

sect.43.3.2 Getting a MAC Address

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply