How do I set the ENET_REF_CLK rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I set the ENET_REF_CLK rate

跳至解决方案
7,010 次查看
michaelworster
Contributor IV

I have a design which uses an i.MX6DL processor, my base design makes use of the Ethernet in RMII mode and uses the GPIO_16 to provide the ENET_REF_CLK. Here is the setup from my device tree:

&fec {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_enet>;
    phy-mode = "rmii";
    phy-reset-gpios = <&gpio5 14 0>;
    fsl,magic-packet;
    status = "okay";
};

What I'm seeing is the Ethernet clock is running at 125MHz and I need it running at 50MHz, I was assuming there would be a max-frequency option in the device tree, but I couldn't find any such entry in the fsl-fec.txt file.

Is there a way to limit the clock rate in the device tree?

If not, how should this be handled?

标签 (4)
0 项奖励
回复
1 解答
6,020 次查看
michaelworster
Contributor IV

Based on feedback from Igor it sounds like there's no way, currently, in the code base/device tree to adjust the ENET_REF clock. As such I've developed a patch file (attached) which checks the device tree and, based on phy-mode, will update the clock rate.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
6,021 次查看
michaelworster
Contributor IV

Based on feedback from Igor it sounds like there's no way, currently, in the code base/device tree to adjust the ENET_REF clock. As such I've developed a patch file (attached) which checks the device tree and, based on phy-mode, will update the clock rate.

0 项奖励
回复
6,017 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michael

device tree entries are parsed in  linux/drivers/net/ethernet/freescale/fec_main.c

(function of_property_read_u32()), please also check attached Linux Manual

Chapter 43 Fast Ethernet Controller (FEC) Driver. Seems RMII mode is defined

in uboot, for example one can look at include/configs/mx6slevk.h

#define CONFIG_FEC_XCV_TYPE        RMII

and board file in /board/freescale/mx6sxsabresd/mx6sxsabresd.c

setup_fec(). Reference clock produced by CCM_ANALOG_PLL_ENETn.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
6,017 次查看
michaelworster
Contributor IV

Thanks for your notes Igor. I've been through fec_main.c and I noticed only the following properties:

num-tx-queues

num-rx-queues

stop-mode

wakeup_irq

phy-reset-duration

So I take it by that, you're saying there is no Device Tree property which can be used to set the clock rate? 

Our Ethernet is setup correctly in u-boot, that is we read the ENET_REF_CLK at 50MHz there, but once the kernel initializes it jumps to 125MHz, which is why I was looking in the kernel for notes on how this is selected.

I also did find the information about the CCM_ANALOG_PLL_ENETn register, but I couldn't find in the code where this was done.

I thought perhaps it had to do with the clk_enet_ref_table from arch/arm/mach-imx/clk-imx6q.c

static struct clk_div_table clk_enet_ref_table[] = {
    { .val = 0, .div = 20, },
    { .val = 1, .div = 10, },
    { .val = 2, .div = 5, },
    { .val = 3, .div = 4, },
    { /* sentinel */ }
};

But making adjustments here seemed to have no effect. Do you have another suggestion where I might look for the setting of this register?

0 项奖励
回复
6,017 次查看
igorpadykov
NXP Employee
NXP Employee

seems this could be done with PHY_INTERFACE_MODE_RMII as in mach-imx6ul.c

linux-2.6-imx.git - Freescale i.MX Linux Tree 

0 项奖励
回复