RMII and RGMII interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RMII and RGMII interface

2,669 次查看
niteshsahay
Contributor III

Hi

I am having a general question regarding RMII and RGMII interface as we have one requirement.

  • In RMII interface , MAC to MAC interface is possible or not.
  • For RGMII , MAC to MAC interface is possible or not

BR\Nitesh

标记 (1)
0 项奖励
回复
1 回复

1,953 次查看
Pavel
NXP Employee
NXP Employee

Look at the following page:

https://community.nxp.com/thread/384125?et=watches.email.thread#610273

See the following documents:

http://www.nxp.com/files/ftf_2010/Americas/WBNR_FTF10_NET_F0568.pdf

and

https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3Fcol...

Tree node and a “fixed-link” property has been added. Details can be found in Documentation/devicetree/bindings/net/fsl-tsec-phy.txt


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复