RGMII to RGMII connection
Hi
In my project i am planning to have MAC to MAC communication (i.e. RGMII) with MCIMX6QP6AVT1AA.
Any idea on how to connect the pins for MAC to MAC communication.
Regards
Nitesh
Look at the following document:
http://www.nxp.com/files/ftf_2010/Americas/WBNR_FTF10_NET_F0568.pdf
Find the "RGMII without a PHY" in this document.
The i.MX6 requires external signal ENET_REF_CLK.
The following connection is needed:
- i.MX6 <=> i.MX6
TXDx => RXDx
RXDx <= TXDx
TX_EN => RX_DV
RX_DV <= TX_EN
TX_ER => RX_ER
RX_ER <= TX_ER
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Is there a better link to the document that is referenced in this topic? The link appears to be broken. I'm looking at using an RGMII to RGMII connection between two i.MX8QM processors - I assume that will work similarly? Also, is there anything special that I need to do regarding the software? Since there is no MDC/MDIO connection I'm guessing there might be.
Thanks so much,
Rich
Hi Pavel
Thanks for the reply.
I am attaching one file can you please help me out in cross verifying the connections i have made for my board (i.e. MAC to MAC).
Another one query regarding TXC and RXC clock i.e. 125MHZ clock will be externally given or how it is?
BR\Nitesh
Yes, External 125 MHz clock source is needed. Find the "RGMII without a PHY" in the following document:
http://www.nxp.com/files/ftf_2010/Americas/WBNR_FTF10_NET_F0568.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel
Thanks for the reply.
One query on Clock:
1) Only single oscillator can be used to generate 125 MHz for TXC and RXC or two different oscillators are used to connect TXC and RXC.
2) Can we have one zero clock delay to generate two output which will be individually connected to TXC and RXC.
BR\Nitesh