Hi Enrique
1.2. "without multimedia framework” means not using video player or other high level
application.
3. from i.MX6DQ RM (for performance of MIPI-CSI2 interface):
The maximum bandwidth of the interface is as follows:
• 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)
for your case, as "16bit RG565 which is acceptable for us. That’s a 168Mpixels/s."
seems this is sufficient.
HDMI is able 1080p60, using kernel parameter video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------