Android or other Linux on the UL, where to start?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android or other Linux on the UL, where to start?

923 Views
claudiohediger
Contributor I

Hi

We have here an i.MX6UL EVK with Display.

We would like to use any kind of Linuxdistribution on it to run our own application.

In the end, the Board should be able to play audiofiles from an SD-Card with our own GUI.

Can anyone tell us, where we can start?

Thanks :smileyhappy:

Labels (1)
0 Kudos
Reply
1 Reply

796 Views
igorpadykov
NXP Employee
NXP Employee

Hi Claudio

linux is more simple, suggest to start with

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul) New

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply