Questions on IPU/DC configuration for 8 bit parallel display bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Questions on IPU/DC configuration for 8 bit parallel display bus

2,371 次查看
dehuanxin
Contributor III

I'm trying to connect a IMX6Q SoC to a LCD display with 8 bit bus, using RGB888 format.

I'm looking at linux-fslc/ipu_disp.c at 3.14-1.1.x-imx · Freescale/linux-fslc · GitHub

My plan is to drive the DC sync wave 3 times faster and use three set of maps to map RGB24 to R8/G8/B8 in each cycle.

To make DC sync clock 3 times faster, I'm planning to change it here.

   rounded_pixel_clk = clk_round_rate(ipu->pixel_clk[disp], pixel_clk);     

   dev_dbg(ipu->dev, "round pixel clk:%d\n", rounded_pixel_clk);     

   ret = clk_set_rate(ipu->pixel_clk[disp], rounded_pixel_clk);     

   if (ret)

   {

        dev_err(ipu->dev, "set pixel clk rate error:%d\n", ret);         

        return ret;     

   }     

   msleep(5);      /* Get integer portion of divider */    

   div = clk_get_rate(clk_get_parent(ipu->pixel_clk_sel[disp])) / rounded_pixel_clk;     

   dev_dbg(ipu->dev, "div:%d\n", div);     

   if (!div)

   {

       dev_err(ipu->dev, "invalid pixel clk div = 0\n");          

       return -EINVAL;     

   }       

   mutex_lock(&ipu->mutex_lock);      

   _ipu_di_data_wave_config(ipu, disp, SYNC_WAVE, div - 1, div - 1);     

   _ipu_di_data_pin_config(ipu, disp, SYNC_WAVE, DI_PIN15, 3, 0, div * 2);

To add additional maps I guess I can do it here

void _ipu_init_dc_mappings(struct ipu_soc *ipu)

What I don't understand is here: how to configure the template to fetch the same RGB24 pixel three times and use 3 different maps to generate three output samples.

Specifically I want to understand what those 4 lines of WROD/WROD/WRG/WROD are doing, especially what's the meaning of "5"?

/* Init template microcode */          

if (disp) {               

    if ((pixel_fmt == IPU_PIX_FMT_YUYV)

        || (pixel_fmt == IPU_PIX_FMT_UYVY)

        ||(pixel_fmt == IPU_PIX_FMT_YVYU)

        || (pixel_fmt == IPU_PIX_FMT_VYUY)) {

        _ipu_dc_write_tmpl(ipu, 8, WROD(0), 0, (map - 1), SYNC_WAVE, 0, 5, 1);

        _ipu_dc_write_tmpl(ipu, 9, WROD(0), 0, map, SYNC_WAVE, 0, 5, 1);

        /* configure user events according to DISP NUM */                    

        ipu_dc_write(ipu, (width - 1), DC_UGDE_3(disp));               

    }

    _ipu_dc_write_tmpl(ipu, 2, WROD(0), 0, map, SYNC_WAVE, 8, 5, 1);

    _ipu_dc_write_tmpl(ipu, 3, WROD(0), 0, map, SYNC_WAVE, 4, 5, 0);

    _ipu_dc_write_tmpl(ipu, 4, WRG, 0, map, NULL_WAVE, 0, 0, 1);

    _ipu_dc_write_tmpl(ipu, 1, WROD(0), 0, map, SYNC_WAVE, 0, 5, 1);

} else {               

     if ((pixel_fmt == IPU_PIX_FMT_YUYV)

         ||(pixel_fmt == IPU_PIX_FMT_UYVY)

         ||(pixel_fmt == IPU_PIX_FMT_YVYU)

         ||(pixel_fmt == IPU_PIX_FMT_VYUY)) {

         _ipu_dc_write_tmpl(ipu, 10, WROD(0), 0, (map - 1), SYNC_WAVE, 0, 5, 1); 

         _ipu_dc_write_tmpl(ipu, 11, WROD(0), 0, map, SYNC_WAVE, 0, 5, 1);       

         /* configure user events according to DISP NUM */

         _ipu_dc_write(ipu, width - 1, DC_UGDE_3(disp));

      }

      _ipu_dc_write_tmpl(ipu, 5, WROD(0), 0, map, SYNC_WAVE, 8, 5, 1);

      _ipu_dc_write_tmpl(ipu, 6, WROD(0), 0, map, SYNC_WAVE, 4, 5, 0);

      _ipu_dc_write_tmpl(ipu, 7, WRG, 0, map, NULL_WAVE, 0, 0, 1);

      _ipu_dc_write_tmpl(ipu, 12, WROD(0), 0, map, SYNC_WAVE, 0, 5, 1);

}

标签 (3)
0 项奖励
回复
1 回复

1,517 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dehuan

WROD/WRG are described in sect.37.4.7.4.1 DC template's memory map

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

it may be helpful to look at some examples with IPU microcode

i.MX53: How to move VGA external HSYNC and VSYNC signals to different pins?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复