Is it possible to use kernel 3.14 with Android Jelly Bean?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use kernel 3.14 with Android Jelly Bean?

855件の閲覧回数
sheldonlrucker
Contributor IV

Due to poor decoding/rendering performance in Android Lollipop our customer has requested that we revert to Jelly Bean.  We've done a fair amount of kernel work in Lollipop that would need to be ported back to Jelly Bean which leads me to the question - is it possible to use kernel version 3.14 with Jelly Bean?

Thank you,

Sheldon

ラベル(3)
0 件の賞賛
返信
1 返信

765件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sheldon

seems this is possible, however one will have to port software,

also gpu drivers provided by nxp with Jelly Bean (L3.0.35) are not compatible

with kernel version 3.14. So with kernel version 3.14 one will have to

use gpu drivers provided with Lollipop.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信