Questions about iMX6 parallel display pixel clock limit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about iMX6 parallel display pixel clock limit

3,495件の閲覧回数
xjgan
Contributor I

     We have a customized imx6q(d) board. To the LCD interface, we found that the larger pixel clock is, more disorder the display will be. This will become obvious when pixel clock goes beyond 40Mhz.

     For an example,  we try to attach a LCD to the parallel RGB port. The LCD parameters are 18bpp(rgb666), 720x1280, 60hz, pixel clock is about 57Mhz. According to the data sheet of the LCD, we set proper timing in the kernel source 'mxc_lcdif.c'. But the display seems to be messed enough.

display_60hz.jpg

     We captured the signal of the DI0_DISP_CLK (pixel clock of RGB signals), the waveform seems mess too.

wave_form_60hz.jpg

     And then, we set the refresh frequency from 60hz to 30hz (in order to downgrade pixel clock without cropping image). Except the refresh frequency, none of the timing items are changed. Then, the display looks good.

display_30hz.jpg      Again, we captured the signal of the DI0_DISP_CLK (pixel clock of RGB signals), the waveform looks clean.

wave_form_30hz.jpg

     We removed LCD from the port, and tried several RGB timing settings with different pixel clocks. Finally, we conclude the result mentioned at the beginning of article. We are using BSP package from 'L3.0.35_1.1.0_121218_source', with patch 03&04 applied. The waveforms of pixel clock are captured from the position most nearby the CPU.

ラベル(3)
0 件の賞賛
返信
1 返信

1,731件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Perhaps the problem relates to the fact, that output IPU pixel clock for LCD may have high jitter.

That's the expected behavior when the clock divider is set to a value that is not an integer.

Please look at IPU hardware parameters Tdicp and Tdpcp in the Datasheet(s).

When the divider is set to a non-integer value, the average frequency of the display clock will be
correct - but the clock will jitter. For applications that are sensitive to jitter, it may be recommended
to apply a clock ratio combination that allowed the clock divider to be set to an integer value.

0 件の賞賛
返信