bitburner not recognized imx233

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitburner not recognized imx233

2,583件の閲覧回数
cesarpantoja
Contributor I

Hi

I have a custom board with imx233, the design has been tested before; but in this, when I prepare to blow fuses with bitburner simply does not recognize it and in the box where it should appear HID ... nothing comes, and I need configure for Boot from SD.

I tried all options in the boot pins and nothing, connectivity also was tested and everything seems in order.

The Bitburner Version and windows version is the same used in other cards equals.

other try to boot from usb with mxsldr but neither recognizes the imx233.

I appreciate any suggestion

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,171件の閲覧回数
Yuri
NXP Employee
NXP Employee

  1. Is it possible to try using BitInit from the OTP TOOLs?

First the otp_burner.py script should be used to generate OtpInit.sb file that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

< https://www.freescale.com/webapp/Download?colCode=IMX_OPT_TOOLS&appType=license&location=null >

2.
As for USB HID detection, please check board USB OTG design :
- if all power voltages meet (i.Mx23) specifications ;
- if USB-5V is present ;
- if the (USB) recovery mode is selected correctly.   

0 件の賞賛
返信

2,171件の閲覧回数
cesarpantoja
Contributor I

Hi Yuri thanks for reply

I found that the voltages are not correct, I checked the decoupling capacitors, but I'm still looking for the cause

0 件の賞賛
返信

2,171件の閲覧回数
Yuri
NXP Employee
NXP Employee

"I found that the voltages are not correct" - so it makes sense to analyze power supply system.

0 件の賞賛
返信