Questions about ddr_stress_tester etc.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about ddr_stress_tester etc.

ソリューションへジャンプ
1,522件の閲覧回数
Hitoshi_Oyama
Contributor I

I have questions about ddr_stress_tester etc.

The specifications of the product under development are as follows

 i.MX6ULL : MCIMX6Y2CVM08AB
 DDR3L : MT41K256M16TW-107AAT x2pcs
  Row : A0-A14 (15bit)
  Bank : BA0-BA2 (3bit)
  Column : A0-A9 (10bit)
  32M x 16 x 8banks = 512MB x2pcs
  Controlled by CS0 and CS1

 

(1)There are various "DDR3 Script Aid", but what should I use?


The following is a question about setting "ddr_stress_tester_v3.00".
(2)What kind of value should be set for MR1 Value? 
 Should I use the value of "MDC0_MDSCR / 0x021b001c" in the generated script? 

(3)Since CS0 and CS1 are used for the connection in the circuit diagram, is it correct to select "ALL" for the "DDR CS" setting? 

0 件の賞賛
返信
1 解決策
1,511件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Hitoshi_Oyama 
Hello,

   please look at my comments below.

1.
    Use the following script

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6ULL-DDR3-Script-Aid/ta-p/1127297?at...

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6ULL-DDR3-Script-Aid/ta-p/1127297

2.
  "The MR1 value can be located on the following line on the initialization script.
The value is the two most significant bytes after the ‘=’ sign, i.e. 0x0004 on this example.


setmem /32 0x021b001c = 0x00048031 // MMDC0_MDSCR, MR1 write, CS0"

 3.
  Yes, it is correct to select "ALL" for the "DDR CS" setting.

 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,512件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Hitoshi_Oyama 
Hello,

   please look at my comments below.

1.
    Use the following script

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6ULL-DDR3-Script-Aid/ta-p/1127297?at...

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6ULL-DDR3-Script-Aid/ta-p/1127297

2.
  "The MR1 value can be located on the following line on the initialization script.
The value is the two most significant bytes after the ‘=’ sign, i.e. 0x0004 on this example.


setmem /32 0x021b001c = 0x00048031 // MMDC0_MDSCR, MR1 write, CS0"

 3.
  Yes, it is correct to select "ALL" for the "DDR CS" setting.

 

Regards,
Yuri.

0 件の賞賛
返信
1,487件の閲覧回数
Hitoshi_Oyama
Contributor I

Hello, Yuri

Thank you for your comments.

I will follow your advice.