I have questions about ddr_stress_tester etc.
The specifications of the product under development are as follows
i.MX6ULL : MCIMX6Y2CVM08AB
DDR3L : MT41K256M16TW-107AAT x2pcs
Row : A0-A14 (15bit)
Bank : BA0-BA2 (3bit)
Column : A0-A9 (10bit)
32M x 16 x 8banks = 512MB x2pcs
Controlled by CS0 and CS1
(1)There are various "DDR3 Script Aid", but what should I use?
The following is a question about setting "ddr_stress_tester_v3.00".
(2)What kind of value should be set for MR1 Value?
Should I use the value of "MDC0_MDSCR / 0x021b001c" in the generated script?
(3)Since CS0 and CS1 are used for the connection in the circuit diagram, is it correct to select "ALL" for the "DDR CS" setting?