Questions about System calibration template of surround view application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Questions about System calibration template of surround view application

623 次查看
Jay_Jiang
Contributor I

Hi,

In “Surround View Application Reference Manual ”, "4.2 System calibration template", Figure 13 shows  Extrinsic camera parameters’ calibration pattern. From this figure,  it seems that the "Poster Height "  could be different from the "Poster Width". If so, the calibration pattern would be a rectangle. 

However, from the source code of SVA, seems that SVA requires the calibration pattern be square( with equal poster height and width).

So my question is, 

Can the  Extrinsic camera parameters’ calibration pattern poster be rectangle,

or it has to be square?

 

Regards,

Jay

 

 

 

0 项奖励
回复
1 回复

588 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @Jay_Jiang 

The calibration pattern can be a rectangle, it is not limited to square.

B.R

0 项奖励
回复