Questions about System calibration template of surround view application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about System calibration template of surround view application

606件の閲覧回数
Jay_Jiang
Contributor I

Hi,

In “Surround View Application Reference Manual ”, "4.2 System calibration template", Figure 13 shows  Extrinsic camera parameters’ calibration pattern. From this figure,  it seems that the "Poster Height "  could be different from the "Poster Width". If so, the calibration pattern would be a rectangle. 

However, from the source code of SVA, seems that SVA requires the calibration pattern be square( with equal poster height and width).

So my question is, 

Can the  Extrinsic camera parameters’ calibration pattern poster be rectangle,

or it has to be square?

 

Regards,

Jay

 

 

 

0 件の賞賛
返信
1 返信

571件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @Jay_Jiang 

The calibration pattern can be a rectangle, it is not limited to square.

B.R

0 件の賞賛
返信