Question on i.MX6 errata document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on i.MX6 errata document

989 Views
t_kuha
Contributor I

I have a question on the latest i.MX6 errata (Rev.7; https://www.nxp.com/docs/en/errata/IMX6DQCE.pdf).

In "Workaround" section of ERR010822 (p.221), the document says "For a non-ISO transfer, the host will discard the packet and the data is lost."

On the other hand, however, in "Description" section, the document says "For an ISO transfer, the packet will be lost."

Now the question is: which description is correct?

(My guess that is "For a non-ISO transfer" in "Workaround" section should be "For an ISO transfer.")

Best regard,

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

890 Views
igorpadykov
NXP Employee
NXP Employee

Hi t_kuha

you are right: "For an ISO transfer, the packet will be lost."

"For a non-ISO transfer, the device will retransmit the packet per the USB specification requirements.."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply