How copy SD card content of Windows CE 5 based embedded system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How copy SD card content of Windows CE 5 based embedded system

2,559 次查看
rezalalechini
Contributor I

I have 2 windows CE 5 embedded system which use i.Max31 application processor, which one is healthy and another one is damaged.

The damaged device have a booting problem and it freeze in booting section.

As i know a problem is SD corruption i tried to do exact copy of SD card from healthy device regarding below link.

https://computers.tutsplus.com/articles/how-to-clone-your-raspberry-pi-sd-cards-with-windows--mac-59...

then wrote this image to the new SD card but it dose not work which any of 2 devices.

how can i solve this problem? and what is the right solution? 

标签 (1)
0 项奖励
回复
1 回复

2,312 次查看
b36401
NXP Employee
NXP Employee

I have no idea what may go wrong with coping.
Please try to use windd utility instead.

Or it is better to use dd utility on Linux PC.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复